Motion

Spray Bottles

Spray bottles can be filled with a wide range of cleaning products, like window cleaning solutions or bathroom cleaners. The user can spray the cleaning solution onto surfaces to clean. Find bottles, trigger sprayers, and bottles with sprayers used for a variety of cleaning applications. A spray bottle is a bottle that consists of a receptacle for storing liquid, along with a handle at the top featuring a trigger-style spray system. A long straw is usually attached to the handle and inserted into the center of the bottle to suck up fluid. When the user presses the trigger, some of the liquid is drawn up the straw and sprays out.